Interfacing Async NAND with iMX6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Interfacing Async NAND with iMX6Q

跳至解决方案
1,434 次查看
atillametetured
Contributor V

Greetings,

We are prepearing a custom HW with an Async Single Die Nand Flash and eMMC. By looking at Sabre for Smart Devices schematics, it is easy to figure out the eMMC connection. We used the  same connections as Sabre did. However looking at Sabre AI board for NAND connections, I cant figure where W/R#, CLK/WE# and WP# pins of the NAND Flash should go. Are they meant for GPIO or do they have a designated connection point on imx?

Thanks in advance

Mete

标签 (2)
0 项奖励
回复
1 解答
1,312 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

these signals can be found in Table 29-1. GPMI External Signals

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,313 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

these signals can be found in Table 29-1. GPMI External Signals

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,312 次查看
atillametetured
Contributor V

Hello Igor,

Thank you. I will consider the manual.

Regards,

Atilla

0 项奖励
回复