Interface ADV7513 with imx7d L_4.9.11

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interface ADV7513 with imx7d L_4.9.11

813 Views
deven_solanki
Contributor III

Hi community,

I am working on imx7d sabresd board with Linux_4.9.11 and I am newbie to HDMI. I want to use HDMI transceiver ADV7513 instead of SiI9022. I have two driver for adv7513 which is using v4l2 and drm framework. But in default bsp we are not using any framework(may be I am wrong). So how can I integrate driver for adv7513 ? Which framework should I used ?

I found that we have also drm driver for SiI902 chip but we are not using it.

 

Thanks & regards.

Solanki Deven

Labels (1)
Tags (1)
0 Kudos
1 Reply

590 Views
igorpadykov
NXP Employee
NXP Employee

Hi Deven

one can try to port new driver using

ADV7511 HDMI transmitter Linux Driver [Analog Devices Wiki] 

and description of nxp hdmi driver in attached Linux Manual  Chapter 15

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos