Intel Centrino Advanced N 6235 bringing up in i-MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Intel Centrino Advanced N 6235 bringing up in i-MX6Q

4,509 Views
balashanmugam
Contributor III

Hi,

                We are using imx6-q7 module with intel centrino advanced N 6235 wifi pcie module in our project and running in linux 3.0.35 kernel. As Intel 6235 module driver  supports from 3.2+ kernel, we have downloaded backport driver iwlwifi (3.10, 3.14) from link (http://wireless.kernel.org/en/users/Drivers/iwlwifi). While loading this driver we are unable to initialize the device. When we analyzing the logs we came to know that the driver tries to send firmware from DRAM to NIC - and NIC doesn’t receive data. 

 

iwlwifi 0000:07:00.0: L1 Disabled; Enabling L0S

iwlwifi 0000:07:00.0: Radio type=0x2-0x1-0x0

iwlwifi 0000:07:00.0: Failed to load firmware chunk!

iwlwifi 0000:07:00.0: Could not load the [0] uCode section

iwlwifi 0000:07:00.0: Failed to run INIT ucode: -110

iwlwifi 0000:07:00.0: Unable to initialize device.

 

I have attached detailed log  for your reference. Could you please help us to fix this issue.

 

Note:

While taking the attached log we have enabled debug=0xffffffff

Original Attachment has been moved to: iwlwifi_debug_logs.txt.zip

Labels (6)
13 Replies

3,177 Views
balashanmugam
Contributor III

Hi,

  Thanks Zhu, Intel 6300 is working thanks for the support, We have faced interrept issue, we disable the MSI interrept, and WIfi works fine now, now we are trying to support WIFI direct and hotspot function.

Regards,

Bala.D

0 Kudos
Reply

3,177 Views
balashanmugam
Contributor III

Hi,

     We have enabled the driver iwlagn driver, we got the following error,

<6>iwlagn: Intel(R) Wireless WiFi Link AGN driver for Linux, in-tree:d

<6>iwlagn: Copyright(c) 2003-2011 Intel Corporation

<6>iwlagn 0000:07:00.0: Detected Intel(R) Centrino(R) Ultimate-N 6300 AGN, REV=0x74

<6>iwlagn 0000:07:00.0: device EEPROM VER=0x436, CALIB=0x6

<6>iwlagn 0000:07:00.0: Device SKU: 0Xb

<6>iwlagn 0000:07:00.0: Valid Tx ant: 0X7, Valid Rx ant: 0X7

<6>iwlagn 0000:07:00.0: Tunable channels: 13 802.11bg, 24 802.11a channels

<6>iwl4965: Intel(R) Wireless WiFi 4965 driver for Linux, in-tree:

<6>iwl4965: Copyright(c) 2003-2011 Intel Corporation

<6>iwlagn 0000:07:00.0: loaded firmware version 9.193.4.1 build 19710

<7>ieee80211 phy0: Selected rate control algorithm 'iwl-agn-rs'

<3>iwlagn 0000:07:00.0: Could not load the INST uCode section

<3>iwlagn 0000:07:00.0: Failed to run INIT ucode: -110

<3>iwlagn 0000:07:00.0: Unable to initialize device.

<3>iwlagn 0000:07:00.0: Could not load the INST uCode section

<3>iwlagn 0000:07:00.0: Failed to run INIT ucode: -110

<3>iwlagn 0000:07:00.0: Unable to initialize device.

Can you please help us to solve this issue.

Note:

     During this testing, we have enabled msi interrupt.

Regards,

Bala.

0 Kudos
Reply

3,177 Views
b47504
NXP Employee
NXP Employee

Which ucode firmware are you using?

0 Kudos
Reply

3,177 Views
balashanmugam
Contributor III

Hi Yuan,

     We have tried iwlwifi-6000g2b-ucode-18.168.6.1.tgz and iwlwifi-6000g2a-ucode-17.168.5.1.tgz u-code.

Driver is able to read iwlwifi-6000g2b-ucode-18.168.6.1.tgz u-code only.

Regards

Arulpandiyan Vadivel

0 Kudos
Reply

3,177 Views
b47504
NXP Employee
NXP Employee

Can the card work on PC using the ucode? Which software release version  you are using?

0 Kudos
Reply

3,177 Views
balashanmugam
Contributor III


We  have not tested this card in PC. We are using backport driver of iwlwifi from 3.10.

Regards

Arulpandiyan V

0 Kudos
Reply

3,177 Views
balashanmugam
Contributor III

We tried intel 6200 wifi card, with its firmware even it fails to come up. It gives the same error.

Regards,

Arulpandiyan V

0 Kudos
Reply

3,177 Views
b47504
NXP Employee
NXP Employee

As you know, we should have released 3.10.17 ga version for imx6. You'd better try to enable it on that bsp firstly. Then we can stay on the same page for the source code. Or I do not know where you modified for the 3.0.5 code to align the code and the log you provided.  

0 Kudos
Reply

3,177 Views
balashanmugam
Contributor III

Sorry for the late reply,

Os Version = 3.0.35

Android = JB 4.2

1. We have tried to enable the CONFIG_IWLMVM and CONFIG_IWLMVM items in kernel config file. But there is no state change.

2. We have patched the pcie.c file in our kernel as per zhu's recommendation to enable the pcie switch(pericom) support.

pci_connections.png

3. We have connected our wifi device as above diagram in our target.

     3.1 We have tried to bring up following wifi devices

          1.intel 6235(DMA issue)

          2.intel 6200(DMA issue)

          3. Atheros 9280(Wlan0 link not ready)

       and all these three devices are not working.

Could you please suggest any of the pcie wifi device(dual band support) which is compatable with imx6 processor in  linux 3.0.35.

Regards

Bala.

0 Kudos
Reply

3,177 Views
b47504
NXP Employee
NXP Employee

According to i.MX_6Dual6Quad_Linux_referece_Manual.pdf, Iwl6300 mini-PCIe wifi card should have been tested:Capture1.JPG.jpg

And here is one link using iwl4965 pcie wifi card on android 4.2:

     https://community.freescale.com/docs/DOC-94045

0 Kudos
Reply

3,177 Views
balashanmugam
Contributor III

Hi,

   can you please tell me the linux version, ours is 3.0.35.

0 Kudos
Reply

3,177 Views
b47504
NXP Employee
NXP Employee

For 6300, the document released together with ltib, it should be 3.0.35 kernel version. I have no the device to try it on my side. You can enable the device config item and locate the firmware to the right path to try it. 

For 4965, it is for JB4.2 ga release, we can apply the patch set directly, I have validated it, and it surely can work.

3,177 Views
b47504
NXP Employee
NXP Employee

Can you enable CONFIG_IWLMVM and CONFIG_IWLMVM items in kernel config file, and then take one try?

0 Kudos
Reply