Integration of LCD on MCIMX6UL-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Integration of LCD on MCIMX6UL-EVK

1,466件の閲覧回数
embedded_Dev
Contributor III

Hi

I am using an MCIMX6UL processor EVKB board and I want to integrate   AFY1024600A0-7.0INTH-R LCD on this processor. Please let me know the procedure..

ラベル(3)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,459件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello mdshami464,

In case of LCD, For developers wishing to use LCD, NXP provides an optional LCD module LCD8000-43T which has a 4.3 inch touch-screen and supports a resolution of up to 480X3(RGB)X272. This module already contains a 50-pin FPC cable, which can be inserted to connector J901 on the base board (the bottom contact). The developer can purchase the LCD module from the NXP website. Now if you have a different LCD make sure that you have 50pin FPC cable to connect to it, and you have develop you own driver to it.

 

Regards

 

0 件の賞賛
返信

1,453件の閲覧回数
embedded_Dev
Contributor III

Hello Bio_TICFSL,

I want know the procedure for integrating LVDS LCD. I know the EVKB is having RGB interface. I am already having LCD. So Can u please share me the procedure.

0 件の賞賛
返信