Integrate LVDS for custom board for imx8qxpc0mek [ O.S Linux Yocto kernel -6.6.3 ] Nanbield.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Integrate LVDS for custom board for imx8qxpc0mek [ O.S Linux Yocto kernel -6.6.3 ] Nanbield.

665件の閲覧回数
Ram2
Contributor III

Hi NXP Team 

Need reference example for LVDS Display on M4 expersso SDK for custom LVDS display for imx8qxpc0mek
We need to example , can you please help us to integrate 

Custom Board : Imx8qxpC0mek [Hardware]
Linux Version :   kernel 6.6.3
SCFW : 1.15
M4 SDK : Xperesso 
Yocto version : Nanbield
Display :  LVDS [ LVDS display is connected via FPC cable between imx8qxp processor and Display ].  


Requirement:
We need to bring up the LVDS display from M4 once target gets turn ON with NXP logo.


How to proceed and where to look in to start any pointers or reference please help us on it.


0 件の賞賛
返信
2 返答(返信)

617件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

For the SDK you may try with dpu driver examples located at <SDK installation path>\boards\mekmimx8qx\driver_examples\dpu

All documentation is available inside the SDK package at <SDK installation path>\docs

Also, note that we do not use an specific driver for a display we just write display timings and other configurations as you will see in all our examples.

You may download SDK from here:
https://mcuxpresso.nxp.com/en/welcome

Best regards/Saludos,
Aldo.

0 件の賞賛
返信

628件の閲覧回数
Ram2
Contributor III

Hi NXP Team,

Any update on below query?


タグ(1)
0 件の賞賛
返信