Integrate 88W9098 BT function to iMX8MPlus L5.4.70.2.3.0 but test bt fail.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integrate 88W9098 BT function to iMX8MPlus L5.4.70.2.3.0 but test bt fail.

Jump to solution
1,532 Views
charleshuang
Senior Contributor II

Hi NXP

We try to Integrate 88W9098 BT function to iMX8MPlus L5.4.70.2.3.0 , but test bt fail.

AIW-WIFI6_9098.jpg

The BT driver is PCIE-UAPSTA-UART-BT-9098-U16-X86-17.68.1.p38-17.26.1.p38-MXM4X17222.P1_V0V1-GPL.

Our platform is iMX8MPlus (ARM64).

Do you have any idea for the fixed issue?

Thanks

0 Kudos
Reply
1 Solution
1,525 Views
igorpadykov
NXP Employee
NXP Employee

Hi Charles

 

for that chip may be recommended to try latest Linux 5.10.35_2.0.0 BSP, described on

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
825 Views
danishv
Contributor I

Hi Did you able build driver for 5.4 kernal ?

0 Kudos
Reply
1,526 Views
igorpadykov
NXP Employee
NXP Employee

Hi Charles

 

for that chip may be recommended to try latest Linux 5.10.35_2.0.0 BSP, described on

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 Kudos
Reply
1,492 Views
charleshuang
Senior Contributor II

Hi NXP Team

 

Our customer need to porting 88w9098 in Yocto3.0  L5.4.70 kernel.

Do you have any idea for porting 88w9098 in Yocto3.0?

0 Kudos
Reply