Integrate 88W8997 BT function to iMX8MPlus L5.4.70.2.3.0 but compiler fail.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integrate 88W8997 BT function to iMX8MPlus L5.4.70.2.3.0 but compiler fail.

1,176 Views
charleshuang
Senior Contributor II

Hi NXP 

We try to Integrate 88W8997 to iMX8MPlus - Yocto3.0 -L5.4.70.2.3.0.

The BT function is not work.

Where I can get the driver for NXP 88W8997 BT (for iMX8MPlus Yocto 3.0)? 

Because Our BT driver is not correct (make fail).

The bt driver link.

PCIE-WLAN-UART-BT-8997-U16-X86-W16.68.10.p16-16.26.10.p16-C4X16640_V4-GPL.zip

And please provide the test BT command for NXP 88W8997.

example:

# hciattach /dev/ttymxc2 any 115200 flow

# hcitool -i hci0 scan

 

0 Kudos
Reply
2 Replies

1,174 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

L5.4.70_2.3.0 for i.MX8MP-EVK supports 88W8997 wifi/bt. you can find related descripitions in i.MX_Linux_Users_Guide.pdf.

See below, please!

weidong_sun_0-1627547865774.png

weidong_sun_1-1627547893119.png

so you don't need to re-compile 8997 driver.

 

try it, please!

Have a good day!

Regards,

weidong

0 Kudos
Reply

1,131 Views
charleshuang
Senior Contributor II

Hi  Weidong_sun

Thanks for your help.

The Question can closed it.

0 Kudos
Reply