Installing libimxvpuapi for imx6q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing libimxvpuapi for imx6q

ソリューションへジャンプ
2,029件の閲覧回数
girijapretha
Contributor II

Hi,

I am trying to install libimxvpuapi library for imx6q. I got the package from below link

GitHub - Freescale/libimxvpuapi: i.MX VPU API Library 

When I try to configure through ./waf command, it is failing with below message,

using the vpulib backend
Checking for library vpu : not found
The configuration failed.

Can you please guide me with steps for installing above package.

Thanks in advance.

ラベル(4)
0 件の賞賛
返信
1 解決策
1,719件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello girijapretha,

You are using a non hardware videos acceleration processor (VPU). or you have no activate the  VPU support on the kernel.

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,720件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello girijapretha,

You are using a non hardware videos acceleration processor (VPU). or you have no activate the  VPU support on the kernel.

Regards

0 件の賞賛
返信
1,719件の閲覧回数
girijapretha
Contributor II

Thanks Bio_TICFSL.

I enabled vpu as part of buildroot and now I am able to install the package.

0 件の賞賛
返信