Installing debian on imx6UL evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installing debian on imx6UL evk

Jump to solution
3,655 Views
pratyushtomar
Contributor IV

I have already tried yocto on imx6UL evk successfully. Now I want to try installing console based debian on imx6UL evk. Is their any ready built debian image available for this or any method how to build and install debian linux on imx6UL evk?

Labels (2)
1 Solution
2,207 Views
Yuri
NXP Employee
NXP Employee

Hello,

    The following may be useful

Debian on the i.MX6 sabre sd platform in a few commands

Debian Jessie Rootfs

Debian Jessie on i.MX6

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,208 Views
Yuri
NXP Employee
NXP Employee

Hello,

    The following may be useful

Debian on the i.MX6 sabre sd platform in a few commands

Debian Jessie Rootfs

Debian Jessie on i.MX6

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,207 Views
cyriacdevasia
Contributor I

I found this site helpful. Followed the instructions (which are remarkably concise and clear) and have debian running on iMX6UL-EVK board.

MCIMX6UL-EVK - Linux on ARM - eewiki 

0 Kudos
Reply