Installing a new OS into i.Mx515

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing a new OS into i.Mx515

931件の閲覧回数
victorwokili
Contributor I

victor wokili asked1 week ago Hello all, I am a novice with putting an OS on a board. So I would like to get a guide on how to flash a new OS.The current OS that's installed is Windows CE 6. The OS I am trying to flash is either Linux BSP L3.0.35v or Android KitKat 4.4.2. In summary, I am trying to : Get a detailed guide on installing Linux BSP L3.0.35v or Android KitKat 4.4.2 (what windows software to use, steps to take) Thank You for your time

ラベル(4)
0 件の賞賛
1 返信

665件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Victor Wokili,


I see that you have received a couple of answers on this topic already. Unfortunately, there is no documentation or support for the i.MX515 on the L3.0.35 Linux BSP or on the Android KK 4.4.2 BSP. This means there is not a step-by-step guide that can be provided.

Regarding Linux my recommendation would be using the Community BSP, which can be downloaded following the instructions on the link below:

http://freescale.github.io/

You could also try using the old L3.0.35 BSP mentioned on the following thread. However, support for LTIB would be much harder to come by than support for Yocto, which has a big community.

https://community.nxp.com/message/1050577

This BSP does support some older boards like the NXP i.MX51 Evaluation Kit and it supports various kernel versions.
As for Android the porting of Kit Kat 4.4.2 to the i.MX515 would be a bit more complicated. You could take Android KK BSP for another board (from NXP or a third party) and work on the necessary porting for the i.MX515, which would require good knowledge on the hardware of the i.MX515 and of Android.

My apologies for the inconvenience. I hope this helps!
Regards,

0 件の賞賛