Installing a new OS into i.Mx515

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installing a new OS into i.Mx515

892 Views
victorwokili
Contributor I

victor wokili asked1 week ago Hello all, I am a novice with putting an OS on a board. So I would like to get a guide on how to flash a new OS.The current OS that's installed is Windows CE 6. The OS I am trying to flash is either Linux BSP L3.0.35v or Android KitKat 4.4.2. In summary, I am trying to : Get a detailed guide on installing Linux BSP L3.0.35v or Android KitKat 4.4.2 (what windows software to use, steps to take) Thank You for your time

Labels (4)
0 Kudos
1 Reply

626 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Victor Wokili,


I see that you have received a couple of answers on this topic already. Unfortunately, there is no documentation or support for the i.MX515 on the L3.0.35 Linux BSP or on the Android KK 4.4.2 BSP. This means there is not a step-by-step guide that can be provided.

Regarding Linux my recommendation would be using the Community BSP, which can be downloaded following the instructions on the link below:

http://freescale.github.io/

You could also try using the old L3.0.35 BSP mentioned on the following thread. However, support for LTIB would be much harder to come by than support for Yocto, which has a big community.

https://community.nxp.com/message/1050577

This BSP does support some older boards like the NXP i.MX51 Evaluation Kit and it supports various kernel versions.
As for Android the porting of Kit Kat 4.4.2 to the i.MX515 would be a bit more complicated. You could take Android KK BSP for another board (from NXP or a third party) and work on the necessary porting for the i.MX515, which would require good knowledge on the hardware of the i.MX515 and of Android.

My apologies for the inconvenience. I hope this helps!
Regards,

0 Kudos