Installing QT 5 or above in Ltib L3.0.35_4.1.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing QT 5 or above in Ltib L3.0.35_4.1.0

ソリューションへジャンプ
1,286件の閲覧回数
nishad_kamdar
Contributor IV

Hi,

I have a custom iMX6q board running with L3.0.35_4.1.0 kernel. I am using Ltib. I have added qt4.6.0 to it and i am able to run a few applications,

However now I am trying to install QT 5 or above in Ltib L3.0.35_4.1.0

Can anyone tell me a procedure how to do it.

regards,

nishad

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
1,037件の閲覧回数
LeonardoSandova
Specialist I

There are two ways to archive this:

Either with Yocto (There is already a layer with all configs done for you, meta-qt5) or cross-compiling against a LTIB rootfs. For the primer, please follow the meta-freescale distribution list, for the latter there is a page on the community, look for 'qt5' results (https://community.freescale.com/docs/DOC-94066?).

Leo

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,038件の閲覧回数
LeonardoSandova
Specialist I

There are two ways to archive this:

Either with Yocto (There is already a layer with all configs done for you, meta-qt5) or cross-compiling against a LTIB rootfs. For the primer, please follow the meta-freescale distribution list, for the latter there is a page on the community, look for 'qt5' results (https://community.freescale.com/docs/DOC-94066?).

Leo

0 件の賞賛
返信