Installing QT 5 or above in Ltib L3.0.35_4.1.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installing QT 5 or above in Ltib L3.0.35_4.1.0

Jump to solution
1,196 Views
nishad_kamdar
Contributor IV

Hi,

I have a custom iMX6q board running with L3.0.35_4.1.0 kernel. I am using Ltib. I have added qt4.6.0 to it and i am able to run a few applications,

However now I am trying to install QT 5 or above in Ltib L3.0.35_4.1.0

Can anyone tell me a procedure how to do it.

regards,

nishad

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
947 Views
LeonardoSandova
Specialist I

There are two ways to archive this:

Either with Yocto (There is already a layer with all configs done for you, meta-qt5) or cross-compiling against a LTIB rootfs. For the primer, please follow the meta-freescale distribution list, for the latter there is a page on the community, look for 'qt5' results (https://community.freescale.com/docs/DOC-94066?).

Leo

View solution in original post

0 Kudos
Reply
1 Reply
948 Views
LeonardoSandova
Specialist I

There are two ways to archive this:

Either with Yocto (There is already a layer with all configs done for you, meta-qt5) or cross-compiling against a LTIB rootfs. For the primer, please follow the meta-freescale distribution list, for the latter there is a page on the community, look for 'qt5' results (https://community.freescale.com/docs/DOC-94066?).

Leo

0 Kudos
Reply