Installing PyEIQ on i.MX 8QuadPlus MEK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Installing PyEIQ on i.MX 8QuadPlus MEK

4,859 次查看
syoganathan
Contributor II

Hello

I would like to install PyEIQ on my i.MX 8QuadPlus MEK eval kit. My Eval board is BO. I installed demo BSP version L5.4.24_2.1.0_MX8QXPB0. The BSP package has "imx-image-multimedia-imx8qxpmek.wic". I created a SD card using this wic file and the board boots up fine.

The PyEIQ installation instruction can be found here  https://pyeiq.dev/1_getting_started/1_1_install_users.html

The installation requires pip3. The BSP "BO" version I installed does not have pip3. It does have python 3.7.

Can someone give me some guidance on how to install PyEIQ on i.MX 8QuadPlus MEK eval kit "BO" version?

Thanks

5 回复数

4,734 次查看
syoganathan
Contributor II

Thank you for the link. My issue is there is no pip3 module on the BSP package L5.4.24_2.1.0_MX8QXPB0 I have installed. The PyEIQ install requires pip3. How can I install pip3 module first.

Thank you

0 项奖励
回复

4,734 次查看
diego_dorta
NXP Employee
NXP Employee

Hi Sivashankar,

You used the multimedia and not the full BSP image, this might be the reason you did not get pip3 installed. Try to use the imx-full-image and let us know.

Please refer to the newest document of PyeIQ: https://community.nxp.com/community/eiq/blog/2020/06/30/pyeiq-a-python-framework-for-eiq-on-imx-proc... 

I also have a suggestion for you, when you have some question related to eIQ I think it would be better if asked on eIQ community, with that it is easier for us to track it :smileygrin:

Thanks,

Diego

4,734 次查看
syoganathan
Contributor II

Hi Diego

That is what I think also. But unfortunately I do not see a full image wic file in BO version of BSP. The CO version of BSP has the full image wic file. My board is a BO board. The BO version  BSP " L5.4.24_2.1.0_MX8QXPB0  " does not have the full image wic file.

Thanks

Shankar

0 项奖励
回复

4,734 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can build by yourself, pls refer to the enclosed file, using "imx-image-full"

0 项奖励
回复

4,734 次查看
joanxie
NXP TechSupport
NXP TechSupport

for eIQ, pls refer to the link as below:

https://community.nxp.com/docs/DOC-346686 

0 项奖励
回复