Installing Apps on Windows 10 IoT Core on i.mx6 Sabre Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing Apps on Windows 10 IoT Core on i.mx6 Sabre Board

3,153件の閲覧回数
sunny_ho
Contributor I

I am able to both build and load the Windows 10 IoT Core ffu onto my i.mx6 sabre board but I'm unable to load any applications. 

Windows 10 IoT Core for i.MX Applications Processors | NXP 

Start->WIndows Device Portal -> Packages only show my installed packages (IoTUAPOOBE and IOTCoreDefaultApplication) but I don't have the ability to load my UWP application (.appxbundle)

What is the best way to load you apps into Windows 10 IoT Core Demo image of the i.mx6 Sabre Board

ラベル(2)
0 件の賞賛
返信
1 返信

3,095件の閲覧回数
art
NXP Employee
NXP Employee

Please follow the general Windows 10 IoT Core documentation for adding application to your Windows 10 IoT Core image:

https://docs.microsoft.com/en-en/windows/iot-core/develop-your-app/appinstaller

Try to add the application to the image as described here:

https://docs.microsoft.com/en-en/windows-hardware/manufacture/iot/deploy-your-app-with-a-standard-bo...

Microsoft claims the method above as the preferred one.

Best Regards,

Artur