Inrush current of i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inrush current of i.MX6DL

1,298 Views
torus1000
Contributor V

Hi chip expert,

We plan to use i.MX6DL for dedicated audio which targeted low power.
So we estimated small power budget but inrush current seems not so few. See *1

How much inrush current typically assumed for i.MX6DL-Sabre-SD board?

Is there any PMIC setting to reduce peak inrush current?

     *1: Large inrush current at boot time on iMX6 SDB
     https://community.freescale.com/message/319035

Thanks.

Labels (2)
0 Kudos
Reply
2 Replies

1,214 Views
art
NXP Employee
NXP Employee

This seems to be the initial power-on current peak when the main power supply is just connected, caused by some massive bypass capacitors charging or something like that. It should not occur on always-powered applications.

Have a great day,

Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,214 Views
torus1000
Contributor V

Dear Artur,

Thank you for replying.

Do you know something how to reduce peak inrush current such as slow Vdd lamp up?

Because if peak current saved less than 2A, we can replace 4A supply to more cheaper 2A one.

Thanks.

0 Kudos
Reply