Inquiry panel DE pad support (innolux,at043tn24) on i.MX6ULL platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inquiry panel DE pad support (innolux,at043tn24) on i.MX6ULL platform

982件の閲覧回数
andychien
Contributor III

Dear Sir,

 

Our customer want to use  innolux,at043tn24 panel on i.MX6ULL platform.

We check RM support below four mode

• MPU Interface
• VSYNC Interface
• DOTCLK Interface
• ITU-R BT.656 Digital Video Interface (DVI)  

 innolux,at043tn24 (attached file) don't have V/H Sync pads and it used DE pad (mode) to control.

We are not sure i.MX6ULL could support it.

Could you help confirm it?

Thanks  

ラベル(1)
0 件の賞賛
返信
1 返信

972件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi andychien

 

yes it can be supported in DOTCLK Mode as described  in Figure 34-13 (signal "ENABLE")

DOTCLK protocol with programmable parameters and Table 34-5. Pin use in DOTCLK Mode

i.MX 6ULL Applications Processor Reference Manual

 

Best regards
igor

0 件の賞賛
返信