Inquiry panel DE pad support (innolux,at043tn24) on i.MX6ULL platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inquiry panel DE pad support (innolux,at043tn24) on i.MX6ULL platform

976 Views
andychien
Contributor III

Dear Sir,

 

Our customer want to use  innolux,at043tn24 panel on i.MX6ULL platform.

We check RM support below four mode

• MPU Interface
• VSYNC Interface
• DOTCLK Interface
• ITU-R BT.656 Digital Video Interface (DVI)  

 innolux,at043tn24 (attached file) don't have V/H Sync pads and it used DE pad (mode) to control.

We are not sure i.MX6ULL could support it.

Could you help confirm it?

Thanks  

Labels (1)
0 Kudos
Reply
1 Reply

966 Views
igorpadykov
NXP Employee
NXP Employee

Hi andychien

 

yes it can be supported in DOTCLK Mode as described  in Figure 34-13 (signal "ENABLE")

DOTCLK protocol with programmable parameters and Table 34-5. Pin use in DOTCLK Mode

i.MX 6ULL Applications Processor Reference Manual

 

Best regards
igor

0 Kudos
Reply