Dear Sir,
Our customer would like use LCD RGB panel to connect i.MX6SL platform.
I checked and found only LCDIF functional description (chapter 21.4 on i.MX6SLRM.pdf).
I reference iMX28 table 33-1 and some pin system mode and vsysnc mode, but don't detail RGB pin connect information.
I provide customer would like use spec. of LCD RGB panel as attachments.
Please help confirm and provide correct connect i.MX6SL pads information.
Thanks a lot,
解決済! 解決策の投稿を見る。
Hi Andy
the R pins should be connected to the most significant bits, then G and finally B.
So for this 24-bit RGB LCD:
R[7:0] <-> LCD_D[23:16]
G[7:0] <-> LCD_D[15:08]
B[7:0] <-> LCD_D[07:00]
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
You could heck the mx6sl-evk schematics for reference. Connector J13 is for a parallel display.
Regards,
Fabio Estevam
Hi Andy
the R pins should be connected to the most significant bits, then G and finally B.
So for this 24-bit RGB LCD:
R[7:0] <-> LCD_D[23:16]
G[7:0] <-> LCD_D[15:08]
B[7:0] <-> LCD_D[07:00]
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------