Inquiry how to connect LCD RGB panel for i.MX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inquiry how to connect LCD RGB panel for i.MX6SL

Jump to solution
940 Views
andychien
Contributor III

Dear Sir,

Our customer would like use LCD RGB panel to connect i.MX6SL platform.

I checked and found only LCDIF functional description (chapter 21.4 on i.MX6SLRM.pdf).

  1. MPU Interface
  2. VSYNC Interface
  3. DOTCLK Interface
  4. ITU-R BT.656 Digital Video Interface (DVI)

I reference iMX28 table 33-1 and some pin system mode and vsysnc mode, but don't detail RGB pin connect information.

I provide customer would like use spec. of LCD RGB panel as attachments.

Please help confirm and provide correct connect i.MX6SL pads information.

Thanks a lot,

Labels (1)
0 Kudos
1 Solution
740 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

the R pins should be connected to the most significant bits, then G and finally B.

So for this 24-bit RGB LCD:

R[7:0] <-> LCD_D[23:16]

G[7:0] <-> LCD_D[15:08]

B[7:0] <-> LCD_D[07:00]

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
741 Views
fabio_estevam
NXP Employee
NXP Employee

You could heck the mx6sl-evk schematics for reference. Connector J13 is for a parallel display.

Regards,

Fabio Estevam

0 Kudos
741 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

the R pins should be connected to the most significant bits, then G and finally B.

So for this 24-bit RGB LCD:

R[7:0] <-> LCD_D[23:16]

G[7:0] <-> LCD_D[15:08]

B[7:0] <-> LCD_D[07:00]

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos