Inquiry about camera interface for i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inquiry about camera interface for i.MX6ULL

477 Views
andychien
Contributor III

Dear Sir,

Our customer want to use 8-bit Camera sensor on i.MX6ULL platform.

Below are they operate a error about planing camera IO pad define by using i.MX  IOMUX tools.

They select CSI_DATA02 to connect camera Y/C[0], but  show CSI_DATA00 (red word is can't use CSI_DATA02)

i.MX6ULLRM.pdf page 746 define T/C[0] is CSI_DATA02.

Please help confirm it.

Thanks, 

snap.jpg

snap1.jpg

Labels (1)
0 Kudos
1 Reply

355 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

seems there is confusion between port name (ipp_csi_d[2]) and pad name - CSI_DATA00,

so for Y/C[0] (signal name DATA2/ipp_csi_d[2])  CSI_DATA00 pad should be selected, as described in RM p.178

pastedImage_3.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos