Inquiry Regarding Debugger and Testing on i.MX 95

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Inquiry Regarding Debugger and Testing on i.MX 95

290 次查看
ThuPham
Contributor I

Hello NXP,

I've some open point with i.MX 95 processor. In the future we will use i.MX 95 in automotive and we may use the i.mx95 for forthcoming project. So we want to find out about debugger, hardware, tools support for i.MX95. So my question is:

1) Which debugger/compiler use for build SW and write the code? If so, Could it run on Windows 10/11 ?

2) Which tools use for flashing SW for i.MX95?

3) What's HW do we need for development and testing?

4) Do you have a roadmap and documentation for i.MX95?

 

Thank you

Thu Pham

 

标记 (1)
0 项奖励
回复
2 回复数

191 次查看
ThuPham
Contributor I

Hi,

Thank you for your information.

0 项奖励
回复

235 次查看
joanxie
NXP TechSupport
NXP TechSupport

i.mx95 is still under preproduction, we don't have much information to share, I only can answer is for imx8 or imx93, imx95 should be similar

1) Which debugger/compiler use for build SW and write the code? If so, Could it run on Windows 10/11 ?

>you can refer to the chapter 2 of enclosed file, which tell you how to compiler the code, Jlink or ARM DS debugger tools

2) Which tools use for flashing SW for i.MX95?

>use UUU tools, for more detailed information, you can refer to this

https://github.com/NXPmicro/mfgtools/releases

3) What's HW do we need for development and testing?

>after launch, we will release the development board for customer testing, you also can order the partner board to test and debug

4) Do you have a roadmap and documentation for i.MX95?
> the plan is that we will release imx95 next year

0 项奖励
回复