Inquiries regarding 4Kp60 signal input of i.MX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inquiries regarding 4Kp60 signal input of i.MX8M

1,392 Views
thankqlee
Contributor I

Inquiries regarding 4Kp60 signal input of i.MX8M

MIMX8MQ6D (8M Quad)

Please inquire about product specifications.
Table 1. Features are marked as follows.
Video Processing Unit
• 4Kp60 HEVC/H.265 main, and main 10 decoder
• 4Kp60 VP9 decoder
• 4Kp30 AVC/H.264 decoder
• 1080p60 MPEG-2, MPEG-4p2, VC-1, VP8, RV9, AVS, MJPEG, H.263 decoder


For the i.MX8M, there is only Two MIPI-CSI for signal input.
Table 1. Looking at the features, does it mean that you can receive 4Kp60 input with Two MIPI-CSI?
When you get input on two MIPIs, you can get 4Kp60 right?


Please review.
I hope you have a warm winter.
thank you.

0 Kudos
Reply
1 Reply

1,385 Views
joanxie
NXP TechSupport
NXP TechSupport

the performance you posted is for vpu, not mipi csi, refer to the reference manual, imx8mq mipi csi performance is:

Support 80Mbps - 1.5Gbps data rate in high speed operation
• Support 10Mbps data rate in low power operation
• Supports 4Kp30, 1080p60/30, 5MP at 15 fps, 720p60, VGA at 60 fps


0 Kudos
Reply