Dear Sir or Madam,
Hello.
I'd like to use the three cameras.
Is it possible to input the three cameras simultaneously i.MX 6Dual or Quad.
OS:Linux
Best Regards,
Keita
解決済! 解決策の投稿を見る。
Hi Keita
in theory it is possible to support up to 4 virtual channels on the MIPI CSI-2 input, refer to
attached file.
One will need to build some aggregator FPGA combining the three separate
camera streams into one with 3 virtual channels.
In general one can use usb camera also.
I think you can find in community IPU x2 cameras solutions (like attached patch), though
I am afraid there are no such for x3 cameras.
Best regards
igor
Hi Keita
in theory it is possible to support up to 4 virtual channels on the MIPI CSI-2 input, refer to
attached file.
One will need to build some aggregator FPGA combining the three separate
camera streams into one with 3 virtual channels.
In general one can use usb camera also.
I think you can find in community IPU x2 cameras solutions (like attached patch), though
I am afraid there are no such for x3 cameras.
Best regards
igor
Hi Igor,
Thank you for your reply.
Is it possible to input from 3 cameras (CSI-1 & CSI-2 & MIPI-CSI) in i.MX6Q?
Best Regards,
Keita
Hi Keita
yes this is possible, in particular
Figure 19-1 "CSI2IPU gasket connectivity" IMX6DQRM
shows data flow for multiple cameras connection.
Best regards
igor