Information of BD-SL-I.mx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Information of BD-SL-I.mx6

818件の閲覧回数
munishsharma
Contributor I

Hi

   I want to record 2 analog  camera's using BD - SL- i.mx6  development board.

     my Question is

     1). can i interface two camera simultaneously on considered board one is connected on MIPI port and other is connected on parallel port and possible to do parallel operation.  

     2). is it possible to stream both camera input on the screen (Hirose DF 14 -20p-1.25H) and store uncompressed both camera input on the sata device.

Thanks in Advance

Regards

Munish

ラベル(1)
0 件の賞賛
返信
1 返信

751件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Munish

in theory both cameras can work concurrently as shows below part

of i.MX6DQ RM

1.jpg

however seems some restrictions exist for that board according to

https://boundarydevices.com/mipi-camera-support-on-i-mx6/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信