Hi
I want to record 2 analog camera's using BD - SL- i.mx6 development board.
my Question is
1). can i interface two camera simultaneously on considered board one is connected on MIPI port and other is connected on parallel port and possible to do parallel operation.
2). is it possible to stream both camera input on the screen (Hirose DF 14 -20p-1.25H) and store uncompressed both camera input on the sata device.
Thanks in Advance
Regards
Munish
Hi Munish
in theory both cameras can work concurrently as shows below part
of i.MX6DQ RM
however seems some restrictions exist for that board according to
https://boundarydevices.com/mipi-camera-support-on-i-mx6/
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------