Information about LPDDR4 installed on i.mx8mdq EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Information about LPDDR4 installed on i.mx8mdq EVK

2,029 Views
DeahyunKim
Contributor II

Thank you in advance for your help.
Q_1: Is LPDDR4 located in EVK discontinued?
Unable to find datasheet for MT53B768M32D4NQ-062 WT:B on Micron site.

Q_2 :If MT53B768M32D4NQ-062 WT:B is discontinued, can I receive the data sheet for the replacement product MT53B768M32D4DT-062 AIT:B?

Q:3 : Is it okay to use MT53B768M32D4DT-062 AIT:B instead of MT53B768M32D4NQ-062 WT:B?
These two memory devices only have a difference in SMD.

Please reply.

Labels (1)
0 Kudos
2 Replies

1,981 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

See below, please!

Q_1: Is LPDDR4 located in EVK discontinued?
No, it is not.  i.MX8MQ supports LPDDR4.

Q_2 :If MT53B768M32D4NQ-062 WT:B is discontinued, can I receive the data sheet for the replacement product MT53B768M32D4DT-062 AIT:B?

yes, you can. MT53B768M32D4DT-062 AIT:B has been used on i.MX8QM-MEK board, so you can also use it on iMX8MQ board.

Q:3 : Is it okay to use MT53B768M32D4DT-062 AIT:B instead of MT53B768M32D4NQ-062 WT:B?
Yes, it is.

 

Have a nice day!

B.R,

weidong

0 Kudos

1,948 Views
DeahyunKim
Contributor II

I have confirmed that MT53B768M32D4DT-062 AIT has been discontinued.

 

Can MT53E768M32D4DT-046 be used as a replacement?

0 Kudos