Info and Development of i.MX6 Sabre Platform for Smart Device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Info and Development of i.MX6 Sabre Platform for Smart Device

4,635件の閲覧回数
andreaalovisi
Contributor I

Hi guys,

I've received this board for exploring the possibility to develop real time applications.

In the box there is a SD card with Android 4.2.2 bootable, so my first question is: Is this board suitable for real time applications?

If yes, i haven't found anywhere info about the flow to follow to develop a linux real time application.

Have you got some hints or tutorial to follow these steps (INCLUDED TOOLS and IDE)? I mean, making a linux bootable card and developing an application targeting the linux platform.

Thank you very much

Regards

0 件の賞賛
返信
6 返答(返信)

4,026件の閲覧回数
andreaalovisi
Contributor I

It's the same,

i'm using ubuntu 14.04 and i tryed both bash and dash shell.

I'm trying to bitabke <image>

but i've got this error:

Schermata del 2015-06-16 13_12_11.png

I verified that if i specify the link in firefox without ";name=ssvb" i succeed in downloading file.
Instead i don't if I keep ";name=ssvb".

I also verified in the .bb file that it contains this line:

Iis there a way to avoid this error?

0 件の賞賛
返信

4,026件の閲覧回数
saurabh206
Senior Contributor III

Hi

Andrea

You can mannualy download these files and put to download folder. also prepare .done file and build again.

Thanks,

Saurabh

0 件の賞賛
返信

4,020件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Andrea

documentation is included in Linux Doc bundle (please look at attached part of it)

L3.14.28_1.0.0_LINUX_DOCS

In general linux is not real time OS

http://bis-linux.com/files/EUF-ENT-T0866_BIS-Embedded_Linux_for_i.MX-Real-World_Projects.pdf

for i.MX6 Linux one can look at RT recipe like linux-imx-rt-3.10.31 on

meta-fsl-arm/recipes-kernel/linux at master · Freescale/meta-fsl-arm · GitHub

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

4,021件の閲覧回数
andreaalovisi
Contributor I

Hi Igor,

Thank you for the answer.

I followed the steps in "Yocto User Guide" and tried to build the image:

5.5 Building an image

The Yocto Project build uses the bitbake command. For example, bitbake <component> builds the named component.

Each component build has multiple tasks, such as fetching, configuration, compilation, packaging, and deploying to the target

rootfs. The bitbake image build gathers all the components required by the image and build in order of the dependency per

task. The first build is the toolchain along with the tools required for the components to build.

The following command is an example on how to build an image:

$ bitbake fsl-image-gui

When i run this command, after a few time, it outputs these error messages:

WARNING: Failed to fetch URL https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-..., attempting MIRRORS if available

ERROR: Fetcher failure: Fetch command failed with exit code 4, no output

ERROR: Function failed: Fetcher failure for URL: 'https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-...'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /home/user/imx6/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/cpuburn-neon/20140626-r0/temp/log.do_fetch.10103

ERROR: Task 2679 (/home/user/sources/meta-openembedded/meta-oe/recipes-benchmark/cpuburn/cpuburn-neon_20140626.bb, do_fetch) failed with exit code '1'

I verified that if i specify the link in firefox without ";name=ssvb" i succeed in downloading file.
Instead i don't if I keep ";name=ssvb".

I also verified in the .bb file that it contains this line:

SRC_URI = "http://hardwarebug.org/files/burn.S;name=mru \

           https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-..."

What if i modify this file and delete the ";name=ssvb"?Or is there another way to avoid this error?

0 件の賞賛
返信

4,021件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Andrea

one can look at tutorial

Freescale Yocto Project main page

~igor

0 件の賞賛
返信

4,021件の閲覧回数
andreaalovisi
Contributor I

Hi Igor,

Thank you for the answer.

I followed the steps in "Yocto User Guide" and tried to build the image:

5.5 Building an image

The Yocto Project build uses the bitbake command. For example, bitbake <component> builds the named component.

Each component build has multiple tasks, such as fetching, configuration, compilation, packaging, and deploying to the target

rootfs. The bitbake image build gathers all the components required by the image and build in order of the dependency per

task. The first build is the toolchain along with the tools required for the components to build.

The following command is an example on how to build an image:

$ bitbake fsl-image-gui

When i run this command, after a few time, it outputs these error messages:

WARNING: Failed to fetch URL https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-..., attempting MIRRORS if available

ERROR: Fetcher failure: Fetch command failed with exit code 4, no output

ERROR: Function failed: Fetcher failure for URL: 'https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-...'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /home/user/imx6/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/cpuburn-neon/20140626-r0/temp/log.do_fetch.10103

ERROR: Task 2679 (/home/user/sources/meta-openembedded/meta-oe/recipes-benchmark/cpuburn/cpuburn-neon_20140626.bb, do_fetch) failed with exit code '1'

I verified that if i specify the link in firefox without ";name=ssvb" i succeed in downloading file.
Instead i don't if I keep ";name=ssvb".

I also verified in the .bb file that it contains this line:

SRC_URI = "http://hardwarebug.org/files/burn.S;name=mru \

           https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-..."

What if i modify this file and delete the ";name=ssvb"?Or is there another way to avoid this error?

0 件の賞賛
返信