Info: Using older mxc_ipudev_test on newer BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Info: Using older mxc_ipudev_test on newer BSP

1,989 Views
StevieRG
Contributor II

Dear all

The previous mxc_ipudev_test supplied in BSP 10.04 contains a lot of very useful sample code and tests which are completely missing from the latest ipudev test. The newer IPU libraries are not completely compatible with the older ipudev tests, so I've made the necessary changes to the older version so it runs with the newer libraries and I've attached it here in case it's useful to others.

Original Attachment has been moved to: 177-1004mxc_ipudev_test.tar.gz

Labels (1)
0 Kudos
Reply
2 Replies

1,370 Views
ela_embedded
Contributor I

Is it possible to convert bayer format into some other formats using this test code ?

0 Kudos
Reply

1,370 Views
fcs
Contributor IV

Freescale doesn't seem to provide this code anymore, so many thanks!

0 Kudos
Reply