Inflexion UI for i.MX Processors not available for download

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inflexion UI for i.MX Processors not available for download

ソリューションへジャンプ
2,163件の閲覧回数
dimitardimitrov
Contributor I

I have an i.MX53 QSB and I would like to download the Inflexion UI for i.MX processors but it is not available either from Mentor Graphics web site:

Inflexion UI for i.MX Processors - Mentor Graphics

or Freescale web site.

The tool should be provided free of charge for use on i.MX processors.

Any help/download link would be highly appreciated.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,781件の閲覧回数
Yuri
NXP Employee
NXP Employee

Inflexion UI for i.MX processors was available free of charge for i.MX51/53

until 1 March 2012.

Mentors Inflexion still supports our processors, but customers need to define

terms directly with Mentor starting 1 March 2012.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,782件の閲覧回数
Yuri
NXP Employee
NXP Employee

Inflexion UI for i.MX processors was available free of charge for i.MX51/53

until 1 March 2012.

Mentors Inflexion still supports our processors, but customers need to define

terms directly with Mentor starting 1 March 2012.

0 件の賞賛
返信
1,781件の閲覧回数
dimitardimitrov
Contributor I

I did contact Mentor Graphics. This is the reply:

Quote:

"Hi Dimitar,

Our Freescale Inflexion program has expired last year, so you would need to purchase Inflexion to use it on your product.

We would need to talk so that I can understand your needs to be able to give you pricing.

We also have Android and Linux experts that can provide Professional Services to help with your design, development or testing.

Please let me know when would be a good time to talk next week or the week after, depending on your timeframe.

Scott".

Mentor's web site also says:

http://www.mentor.com/embedded-software/inflexion/ui-imx-processors

Quote: "Freescale provides this tool and engine free of charge for use on the following processors*:"

0 件の賞賛
返信