Inferencing custom model on NPU of IMX 8M Plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inferencing custom model on NPU of IMX 8M Plus

730 Views
abhishek_ml
Contributor I

We are trying to run MobileNet_v2 model trained on custom dataset for object detection. Generated 'saved_ model.pb' by using export_tflite_graph_tf2.py from TF2-ODAPI

Quantization is done using tflite converter (script attached) method with int8 data type. When the output quantized .tflite is inferenced on IMX 8M Plus  using libvx_delegate, it falls back to CPU.

The details of env/frameworks used:

1. Tensorflow : 2.10.0 

2. TF Lite : 2.10.0

3. Python: 3.8.10

Following combination of input, weight and output were tested:

1. uint8, int8, uint8

2. uint8, int8, float32

3. float32, int8, float32

We were not able to convert weights to uint8 data type as in this model (works with high FPS)

TF Lite runtime on IMX is 2.8.0

For test inferencing gstreamer pipeline from IMX Machine Learning guide is used.

gst-launch-1.0 v4l2src device=/dev/video3 ! video/x-raw,width=640,height=480,framerate=30/1 ! tee name=t t. ! queue max-size-buffers=2 leaky=2 ! imxvideoconvert_g2d ! video/x-raw,width=300,height=300,format=RGBA ! videoconvert ! video/x-raw,format=RGB ! tensor_converter ! tensor_filter silent=false framework=tensorflow2-lite model=./custom_mobilenet_v2.tflite accelerator=true:npu custom=Delegate:External,ExtDelegateLib:libvx_delegate.so ! tensor_decoder silent=false mode=bounding_boxes option1=tf-ssd option2=./custom_labels.txt option3=0:1:2:3,50 option4=640:480 option5=300:300 ! mix. t. ! queue max-size-buffers=2 ! imxcompositor_g2d name=mix sink_0::zorder=2 sink_1::zorder=1 ! autovideosink

 

 

 

 

 

 

 

0 Kudos
3 Replies

700 Views
abhishek_ml
Contributor I

how can we dump the debug log in gstreamer ?

0 Kudos

694 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @abhishek_ml 

Refer the 10.1.2 Profiling on hardware accelerators in ML guide: https://www.nxp.com/docs/en/user-guide/IMX-MACHINE-LEARNING-UG.pdf

Qmiller_0-1670811363253.png

 

0 Kudos

707 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @abhishek_ml 

Please attach the debug log.

0 Kudos