Infer wrong values of bounding box on NPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Infer wrong values of bounding box on NPU

Jump to solution
2,212 Views
MiloJan
Contributor I

Hello NXP,

Our program can use the NPU to achieve acceleration using the tflite VX delegate, but can't obtaine the same result as the CPU.

The label value can be obtained correctly, but the value of the bounding box is always 0.

Our environment:

Board: i.MX 8M Plus EVK

System: kirkstone-5.15.71-2.2.0

Tflite Mode: Yolov v7.0

Is there something we didn't notice?

0 Kudos
Reply
1 Solution
2,034 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MiloJan,

I hope you are doing well.

Please find a response from the engineering team below.

One can use the attached patch to fix the issue on the 5.15.71_2.2.0. Use the Yocto SDK to build the libvx_delegate.so.

The steps are as below:

1. Setup the Yocto SDK 5.15.72.(Refer to the i.MX Yocto Project User's Guide)

2. bitbake the vx_delegate, and use the patch by the command

bitbake tensorflow-lite-vx-delegate

cd imx-yocto-bsp/8mp_5.15.72_2.2.0/build-xwayland/tmp/work/armv8a-poky-linux/tensorflow-lite-vx-delegate/2.9.1-r0/git

git apply diff.patch

bitbake -c compile -f tensorflow-lite-vx-delegate

bitbake -c build -f tensorflow-lite-vx-delegate

the libvx_delegate.so will be generated in ../image/usr/lib/

3.copy the libvx_delegate to the broad path /usr/lib/

Thanks & Regards,
Dhruvit Vasavada

View solution in original post

0 Kudos
Reply
5 Replies
2,114 Views
MiloJan
Contributor I

Hello @Dhruvit ,

How is it. Could you reproduce that?

0 Kudos
Reply
2,035 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MiloJan,

I hope you are doing well.

Please find a response from the engineering team below.

One can use the attached patch to fix the issue on the 5.15.71_2.2.0. Use the Yocto SDK to build the libvx_delegate.so.

The steps are as below:

1. Setup the Yocto SDK 5.15.72.(Refer to the i.MX Yocto Project User's Guide)

2. bitbake the vx_delegate, and use the patch by the command

bitbake tensorflow-lite-vx-delegate

cd imx-yocto-bsp/8mp_5.15.72_2.2.0/build-xwayland/tmp/work/armv8a-poky-linux/tensorflow-lite-vx-delegate/2.9.1-r0/git

git apply diff.patch

bitbake -c compile -f tensorflow-lite-vx-delegate

bitbake -c build -f tensorflow-lite-vx-delegate

the libvx_delegate.so will be generated in ../image/usr/lib/

3.copy the libvx_delegate to the broad path /usr/lib/

Thanks & Regards,
Dhruvit Vasavada

0 Kudos
Reply
1,989 Views
MiloJan
Contributor I

Hello @Dhruvit,

This works for us. Thanks.

 

 

0 Kudos
Reply
2,083 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MiloJan,

I hope you are doing well.

I have reproduced it and I think the root cause is the vxdelegate driver update.

I am checking the two branch differences and the commit log.

I will update here ASAP.

Thanks & Regards,
Dhruvit Vasavada

0 Kudos
Reply
2,187 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MiloJan,

I hope you are doing well.

I am trying to reproduce this issue on my end.

I will get back to you once done.

Thanks & Regards,
Dhruvit Vasavada

 

0 Kudos
Reply