Inconsistency between iMX6 Clock Tree and Clock Root Generator diagrams

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Inconsistency between iMX6 Clock Tree and Clock Root Generator diagrams

跳至解决方案
1,869 次查看
MichaelV
Senior Contributor III

There seems to be an inconsistency between the iMX6SDL CCM Clock Tree diagram (figure 18-3) and the BUS clock generation (diagram (figure 18-5).

  • The BUS clock generation diagram shows a second mux (periph_clk_sel) that is not on the clock tree.
    Please confirm the BUS clock diagram is correct and the Clock Tree diagram is missing this mux

  • The 3rd option on the pre_periph_clk_sel mux shows "PLL2_PFD0 /2" on the BUS clock generation diagram, but on the clock tree this is "PLL2_PFD2 /2"
    Please confirm the correct source is "PLL_PFD2 /2"

  • There is a 3rd mux in the path; burn_in_bist
    Is this a real mux, and if yes; who or what sets burn_in_bist?

标签 (5)
0 项奖励
回复
1 解答
1,408 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Michel

1. BUS clock generation (diagram (figure 18-5) is correct. Figure 18-3 is just simplified figure.

2. Yes, correct is PLL2_PFD2 /2.

3. burn_in_bist is used for factory testing only.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,409 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Michel

1. BUS clock generation (diagram (figure 18-5) is correct. Figure 18-3 is just simplified figure.

2. Yes, correct is PLL2_PFD2 /2.

3. burn_in_bist is used for factory testing only.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复