Including AVS in yocto with custom sound card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Including AVS in yocto with custom sound card

1,102 次查看
ganapathiraopil
Contributor I

Hi,

I am using i.mx7D PicoPi board.

Previously I was tried to build AVS in fsl image locally. But now I found a link which is providing the info to build Alexa SDK using yocto: "https://community.nxp.com/docs/DOC-340189 ".

 

In this image every dependency is added and AVS is working well, but I am unable to add a custom sound card to this  kernel image. I added the corresponding driver files and did the configuration in corresponding Makefile and Kconfig file and in device tree file also.

When I am trying to enable my sound card driver from menuconfig, it is not getting effected in the final image. And the when I am checking back the kernel configuration in menuconfig editor, the driver is deselecting.

When I did this in fsl normal image, the sound card is added successfully and I am able to record the voice.

Help me regarding this..

Thanks in advance..

Regards,

Ganapathirao.

标签 (3)
0 项奖励
回复
0 回复数