In Serial Downloader mode, download using USB, PC does not link to USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In Serial Downloader mode, download using USB, PC does not link to USB

872件の閲覧回数
353533661
Contributor I

In my design, i.mx6ul's UART2_RXD, UART4_RXD, UART5_RXD connected to other MCUs of UART.Internal Boot start-up, i.mx6ul and MCU's UART data communication is no problem.
When in Serial Downloader mode, and this MCU is working, using USB download, the PC does not link to USB.
If the MCU stops working, the PC can link to USB and download it complete.
Is there a BUG in i.mx6ul?

タグ(1)
0 件の賞賛
返信
1 返信

822件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi xiaojun

according to Figure 8-2. Serial Downloader boot flow

i.MX 6UltraLite Applications Processor Reference Manual

both uart and usb are polling by ROM. So uart activity may prevent

PC link to USB.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信