In Lite5200, Linux-3.18.9 fails to assign the Major number to Nor Flash(with uboot-1.2.0)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In Lite5200, Linux-3.18.9 fails to assign the Major number to Nor Flash(with uboot-1.2.0)

Jump to solution
1,073 Views
anilkdevagiri
Contributor I

Kernel command line:

VFS: Cannot open root device "(null)" or unknown-block(0,0): error -6
Please append a correct "root=" boot option; here are the available partitions:
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
Rebooting in 180 seconds..

0 Kudos
Reply
1 Solution
848 Views
anilkdevagiri
Contributor I

It is solved by adding the "chosen" node in device tree.

All the best.

View solution in original post

0 Kudos
Reply
1 Reply
849 Views
anilkdevagiri
Contributor I

It is solved by adding the "chosen" node in device tree.

All the best.

0 Kudos
Reply