In uboot i want to assign a MX6_PAD_EIM_D22__GPIO3_IO22 | ID_PAD_CTRL as a ouput mode so it can supply 3.3v output
How to configure this
/*
#define ID_PAD_CTRL (PAD_CTL_PKE | PAD_CTL_PUE | \
PAD_CTL_PUS_47K_UP | PAD_CTL_SPEED_LOW | \
PAD_CTL_DSE_80ohm | PAD_CTL_SRE_FAST | PAD_CTL_HYS) */
unable to configure this as the output mode to supply 3.3v from this pin,
also may be useful to check macros in uboot/arch/arm/include/asm/arch-mx6
for example uart settings :
static iomux_v3_cfg_t const uart1_pads[] = {
MX6_PAD_CSI0_DAT10__UART1_TX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),
MX6_PAD_CSI0_DAT11__UART1_RX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),
};
http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6sabresd/mx6sabresd.c...
~igor
Hi,
You need to modify board/boundary/nitrogen6x/nitrogen6x.c to add your pin muxing to the init_pads array:
u-boot-imx6/nitrogen6x.c at boundary-v2016.03 · boundarydevices/u-boot-imx6 · GitHub
Then you need to add that pad to the gpios_out_low/high array (depending on which level you want) so U-Boot initializes it:
u-boot-imx6/nitrogen6x.c at boundary-v2016.03 · boundarydevices/u-boot-imx6 · GitHub
Regards,
Gary