Hi,
I am using i.MX 8QuadXPlus MEK CPU Board. i am trying to flash board using yocto project source code .
Image :fsl-image-validation-imx-xwayland-imx8qxpmek.sdcard image by following command. (referred the manual)
sudo dd if=fsl-image-validation-imx-xwayland-imx8qxpmek.sdcard of=/dev/sdb bs=1M conv=fsync
Sdcard partition (Boot partition and rootfs) is created and all the files are copied into it ,but the board is not booting up and i don't see any boot logs
DIP switches are set to SD card boot
I am unable to figure it out what is causing the issue.
Hi Ramesh,
Check, If you are booting for SD1 the SW2 D1,D2 must be ON D3,D4 OFF. if you are on eMMC D3 must be ON all rest
OFF.
Thanks