Imx8qm use MIPI_DSI0_GPIO0_00 as a pwm out pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx8qm use MIPI_DSI0_GPIO0_00 as a pwm out pin

584 Views
smarter
Contributor II

Hi,

 1.  How can I use MIPI_DSI0_GPIO0_00 as a pwm out pin? it seems not implement at imx8qm platform as what LVDS0_GPIO00 does.

2. MIPI DSI only has one clock source ,IMX8QM_MIPI0_PWM0_CLK, how can I implemet device tree as mipi_pwm as lvds0_pwm do.

0 Kudos
1 Reply

557 Views
igorpadykov
NXP Employee
NXP Employee

Hi bin

one can try to develop it using existing LVDS0_GPIO00 pwm as example and

SCFW Porting Kit

https://community.nxp.com/docs/DOC-341481 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos