Imx8mqevk yocto 5.4.70 custom resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx8mqevk yocto 5.4.70 custom resolution

2,935 Views
thinhpham
Contributor I

Hi experts,

I'm using imx8m-evk, I have bought waveshare 7inch hdmi (c) model. This screen supports fixed resolution 1024x600, but from drm/fb0/modes, I could not find this resolution. I can see the nxp logo at boot time, but it does not show the penguin, loading screen and main desktop. I suppose a reason is from not supported resolution in yocto build. How can I add a custom resolution to my build?

Thank you!

0 Kudos
Reply
9 Replies

2,927 Views
joanxie
NXP TechSupport
NXP TechSupport

try to add 1024x600 in the drm_dmt_modes ofdrm_edid.c according to your display spec,

"https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/drm_edid.c?h=imx_5.4.70_2....

after boot up, check the log file if the board detect the display or not

0 Kudos
Reply

2,917 Views
thinhpham
Contributor I

Hi joanxie,

I added several settings in

linux-imx/drivers/gpu/drm/drm_edid.c

 

// In drm_dmt_modes
/* 0x59 - 1024x600@60Hz */
{ DRM_MODE("1024x600", DRM_MODE_TYPE_DRIVER, 54000, 1024, 1072,
	   1168, 1312, 0, 600, 603, 613, 626, 0,
	   DRM_MODE_FLAG_PHSYNC | DRM_MODE_FLAG_NVSYNC) },

// In edid_cea_modes
/* 108 - 1024x600@60Hz 16:9 */
{ DRM_MODE("1024x600", DRM_MODE_TYPE_DRIVER, 54000, 1024, 1072,
	1168, 1312, 0, 600, 603, 613, 626, 0,
	DRM_MODE_FLAG_NHSYNC | DRM_MODE_FLAG_NVSYNC),
	.vrefresh = 60, .picture_aspect_ratio = HDMI_PICTURE_ASPECT_16_9, },

 

sources/meta-imx/meta-bsp/recipes-graphics/wayland/weston-init/weston.ini

 

[output] 
name=HDMI-A-1
mode=1024x600@60

 

But still no 1024x600 resolution in cat /sys/class/drm/card0-HDMI-A-1/modes

Thank you!

0 Kudos
Reply

2,895 Views
joanxie
NXP TechSupport
NXP TechSupport

could you send the log file to me? how did you connect the hdmi to imx8mq board? via dcss or lcdif?

 

0 Kudos
Reply

2,892 Views
thinhpham
Contributor I

Sorry, I'm new to embedded development so could you please tell me which log file do you want to check? Btw, my screen connected to hdmi port on evk board directly.

0 Kudos
Reply

2,888 Views
joanxie
NXP TechSupport
NXP TechSupport

when the board boot up, you should get print information from the uart debug port, send this information to me

 

0 Kudos
Reply

2,883 Views
thinhpham
Contributor I

Hi, sorry for delay. I have struggled to get the log for awhile. Here it is, please check!

0 Kudos
Reply

2,876 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems that this isn't complete log file, pls send the information start of the board boot up

0 Kudos
Reply

2,874 Views
thinhpham
Contributor I

Sorry, I captured the log file again, please check it. Thank you!

0 Kudos
Reply

2,853 Views
joanxie
NXP TechSupport
NXP TechSupport

did you use dcss or lcdif? refer to the log file, you use dcss, right? which dts file do you use? or send your dts file to me

 

0 Kudos
Reply