Imx8mp Andorid 13 Disable DHCP for LAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx8mp Andorid 13 Disable DHCP for LAN

934 Views
shiva141
Contributor II

Hi ,

IMX8MP Andorid 13 we are not able to update the static IP form UI

UI network -> ethernet  configuration -> static IP -> then set static ip , gateway , and then gave save;  we got Response : FAILED TO SAVE NETWORK;

attached logcatd during this activity 

if we update the Static IP from Command line ; within few moment It get auto updated to DHCP IP  

IMX8MPLUS #Andorid 13

How to disable DHCP for LAN from Command line.


 

 

0 Kudos
Reply
1 Reply

912 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

  1. As root, start dhcpconfig by typing the following command: # /usr/sbin/dhcpconfig.
  2. Select Unconfigure DHCP or Relay Service by typing 3 .
  3. Type Y at the following prompt to disable DHCP: Unconfigure will stop the DHCP service and remove /etc/default/dhcp.

Regards

 

0 Kudos
Reply