Imx8mmevk Thermal Critical Temperature shutdown

cancel
Showing results for 
Search instead for 
Did you mean: 

Imx8mmevk Thermal Critical Temperature shutdown

139 Views
santhosh2
Contributor IV

Hello,

we have designed a customized board with imx8mmevk processor and we are testing for thermal shock test from -40 degree C to +85 degree C (Dwell Time is 2 hrs and ramp time is 1 to 3 minute). Under this the processor is shutting it self between +75 degree C to +85 degree C. Please find the attached log

85 degree 23_Jan2021_procecssortrace_1.jpg

how to ensure that the processor doesnt shutdown when this is reaching at 85 degree C

 

Regards

santhosh

0 Kudos
3 Replies

126 Views
b36401
NXP TechSupport
NXP TechSupport

You can configure shutdown temperature in Linux.
Please refer to chapter 2.9 "Thermal" of i.MX Linux Reference Manual.

0 Kudos

117 Views
santhosh2
Contributor IV

Yes I changed as per the settings but the processor CPU temperature is reaching 100 degree C when the environmental chamber temperature is 75 Deg C

cat /sys/devices/virtual/thermal/thermal_zone0/temp 

Used the above command to get the CPU temperature

 

Regards

Santhosh

 

0 Kudos

70 Views
b36401
NXP TechSupport
NXP TechSupport

Please look at the patch in this thread:

https://community.nxp.com/t5/i-MX-Processors/i-mx8mm-cpureq-cooling-issue/m-p/1176540

Maybe it helps.

0 Kudos