#Use Imx8mm to driver 4096*3702@30fps camera when I get stream on , and the console print "base address switching Change Err.",so I check the CSI status register ,and it`s value as follow picture:
I have 2 question:
1.if this chip support this camera resolution.
2.if this camera problem result from DMA could not transform data(about 12M pre frame) in time.
Hi PX_forever
regarding support of "4096*3702@30fps camera", I am afraid it is not supported as MIPI CSI performance
is described in sect.13.1.1 Multimedia Overview i.MX 8M Mini Applications Processor Reference Manual
"Support up to 1080p@60fps video capture"
Best regards
igor