Hi
I have a *MX8 DSI OLED1* display which I want to use with IMX8 Mini. I've started the board with the default os on MMC and loaded the rm67191 dtb from uboot, lcd is showing the image but there is a strange issue with it displaying two colors on the screen as can be seen in the attached image. This is also the case for a custom OS built using Yocto. How can I solve this issue?
Regards.