Imx8 Demo Capacitor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx8 Demo Capacitor

952 Views
FilippoDeveloper
Contributor I

Hi at all,

 

in the demo board and exacly IMX8QM POWER sheet, are reported some pair of capacitor in parallel connection with same value but different work voltage; i saw also the impedance comparison function of frequency but are the same, for example C372 2.2uF 10V and C378 2.2uF 6.3V why this selection? instead to use 2 capacitor of same work voltage? 

Thanks

Filippo

0 Kudos
Reply
2 Replies

936 Views
FilippoDeveloper
Contributor I

Ok, thanks for your reply. I think that double choose possibility was for a new engineering project...perhaps..

Best Regards

Filippo

 

0 Kudos
Reply

941 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

I discussed your question with i.MX Expert. Here are some explanations and suggestions for you:
1. For these capacitors, in your own design, you can choose either 10V or 6.3V according to the output voltage.
2. On the board, for the 3.3V IO power supply, we recommend using a 10V capacitor.

In order to unify the components on the board, we recommend that you use 10V capacitors.

[comment]
For other power supply circuits, all capacitors can be selected according to the power supply output voltage.

 

Hope this information is helpful to you.

Have a nice day!

B.R,

Weidong