Hello All,
I am interfacing imx7d ethernet with DP83825 in RMII mode. My device tree setting is as follows:
I can connect to PHY but, after I check with the ethtool the link is not being detected. I get the following output.
Following the imx7d reference manual, the pin configuration was not clear for me in RMII mode.
Is my pin setting for RMII is correct? Could somebody please confirm pin selection for RMII?
Thanks,
Asma
Hi Asma
for rmii connections one can look at
software rmii example in toradex colibri board
imx7-colibri.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykovโ,
Thanks for the quick reply.
Looking at the above link
RMII interface on the IMX7
looks like pad MX7D_PAD_ENET1_CRS__ENET1_CRS is not right for CRS_DV.
Our hardware engineer said, he is not able to select ENET1.RX_CTL for CRS_DV in Pin Tool for i.Mx.
Could you please confirm, if we can use MX7D_PAD_ENET1_CRS__ENET1_CRS for CRS_DV or not?
Thanks,
Asma
Hi Asma
suggest to try toradex colibri board configuration given above, it works as
CRS_DV in RMII mode inspite of naming.
Best regards
igor
Hi Igor,
toradex colibiri board is using following device tree settings
pinctrl_enet1: enet1grp { fsl,pins = < MX7D_PAD_ENET1_CRS__GPIO7_IO14 0x14 MX7D_PAD_ENET1_RGMII_RX_CTL__ENET1_RGMII_RX_CTL 0x73 MX7D_PAD_ENET1_RGMII_RD0__ENET1_RGMII_RD0 0x73 MX7D_PAD_ENET1_RGMII_RD1__ENET1_RGMII_RD1 0x73 MX7D_PAD_ENET1_RGMII_RXC__ENET1_RX_ER 0x73 MX7D_PAD_ENET1_RGMII_TX_CTL__ENET1_RGMII_TX_CTL 0x73 MX7D_PAD_ENET1_RGMII_TD0__ENET1_RGMII_TD0 0x73 MX7D_PAD_ENET1_RGMII_TD1__ENET1_RGMII_TD1 0x73 MX7D_PAD_GPIO1_IO12__CCM_ENET_REF_CLK1 0x73 MX7D_PAD_SD2_CD_B__ENET1_MDIO 0x3 MX7D_PAD_SD2_WP__ENET1_MDC 0x3 >; };
So that means they are using ENET1.RX_CTL for CRS_DV and we have use ENET1_CRS for CRS_DV. which means we have used the wrong PAD. Is that right?
Could you now confirm that?
Regards,
Asma
Hi Asma
>we have use ENET1_CRS for CRS_DV. which means we have used the wrong PAD. Is that right?
right, actually for CRS_DV Table shows in "Pad" column ENET1.RX_CTL.
Best regards
igor
Thanks igorpadykovโ