Imx6ul whether to support the rndis function and how to set up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6ul whether to support the rndis function and how to set up

1,528件の閲覧回数
liangmu
Contributor I

Dear,

In imx6ul evk baseline,whether to support rndis host ,and how to set up code。

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,367件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi liang

please check

USB Device Mode (Linux) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,367件の閲覧回数
liangmu
Contributor I

Dear igor,

I've read the information you provided, but it's not quite clear yet. I use imx6ul as a host here, want to link a Android mobile phone through the rndis, how to modify the specific?

发件人: igorpadykov

发送时间: 2017年12月22日 7:08

收件人: liang mu

主题: Re: - Re: Imx6ul whether to support the rndis function and how to set up

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

Re: Imx6ul whether to support the rndis function and how to set up

reply from igorpadykov <https://community.nxp.com/people/igorpadykov?et=watches.email.thread> in i.MX Community - View <https://community.nxp.com/message/972105?commentID=972105&et=watches.email.thread#comment-972105> the full discussion

0 件の賞賛
返信