Imx6ul use 1280*800 display, how many frames can be displayed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6ul use 1280*800 display, how many frames can be displayed

1,428 Views
liangmu
Contributor I

Dear ,

I use the imx6ul evk baseline, and the screen resolution is set to 1280*800, and how much is the frame rate set at this time? Will the shadow be displayed?

Labels (1)
0 Kudos
Reply
2 Replies

1,270 Views
joanxie
NXP TechSupport
NXP TechSupport

for hardware side, refer to the material,

  • Display Resolution

Support up to WXGA@60fps with rich UI & application

Support up to 1080p@60fps with limited UI update*

Maximal pixel rate: 150 MP/sec

for the max, you can set 60

for software side, I got document as below:

The LCD driver controller is ili9341, resolution is 320x240, bpp is 16.When SPI bit per word is 32, the performance is 30fps.

so this depends what bpp and what bsp version you use.

0 Kudos
Reply

1,270 Views
liangmu
Contributor I

Thinks for your replay!

In our baseline code,i have find the lcd resolution set to 60fps.

0 Kudos
Reply