Imx6ul use 1280*800 display, how many frames can be displayed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6ul use 1280*800 display, how many frames can be displayed

1,261 Views
liangmu
Contributor I

Dear ,

I use the imx6ul evk baseline, and the screen resolution is set to 1280*800, and how much is the frame rate set at this time? Will the shadow be displayed?

Thinks

0 Kudos
Reply
3 Replies

1,113 Views
igorpadykov
NXP Employee
NXP Employee

Hi liang

as i.MX6UL has not VPU, all codec operations are performed in software

and framerate depends mainly on processor load (use case). In nxp bsps

software codec performance is described in  Table 30. Video codec specification for

hardware without VPU acceleration attached Release Notes, for resolution 1280*800

it may be recalculated accordingly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,113 Views
liangmu
Contributor I

Dear,

"Nxp bsps software codec performance is described in  Table 30",Which document?

0 Kudos
Reply

1,113 Views
igorpadykov
NXP Employee
NXP Employee

document in attachment previous answer (in red).

pastedImage_3.jpg

0 Kudos
Reply