Imx6ul deploy folder files deleted

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6ul deploy folder files deleted

4,018 Views
srinivasulured1
Contributor I

Hi,

I am using imx6ul eval board. I followed the "yocto project user guide" to create the images. but few files are deleted from ~/tmp/delpoy/images/imx6ulevk" folder. when i try to recreate the images i am getting the following error.

WARNING: log_check: There is a warn message in the logfile

WARNING: log_check: Matched keyword: [WARNING:]

WARNING: log_check: WARNING: The license listed Firmware-atheros_firmware was not in the licenses collected for linux-firmware

ERROR: Error: The image creation script '/home/srinivasulu/Freescale_BSP/Build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-base/1.0-r0/temp/create_image.sdcard' returned 1:

0+0 records in

0+0 records out

0 bytes (0 B) copied, 7.8307e-05 s, 0.0 kB/s

Model:  (file)

Disk /home/srinivasulu/Freescale_BSP/Build/tmp/deploy/images/imx6ulevk/core-image-base-imx6ulevk-20151228075336.rootfs.sdcard: 88.1MB

Sector size (logical/physical): 512B/512B

Partition Table: msdos

Disk Flags:

Number  Start   End     Size    Type     File system  Flags

1      4194kB  12.6MB  8389kB  primary               lba

2      12.6MB  83.9MB  71.3MB  primary

dd: failed to open '/home/srinivasulu/Freescale_BSP/Build/tmp/deploy/images/imx6ulevk/u-boot-imx6ulevk.imx': No such file or directory

WARNING: exit code 1 from a shell command.

ERROR: Function failed: do_rootfs

ERROR: Logfile of failure stored in: /home/srinivasulu/Freescale_BSP/Build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-base/1.0-r0/temp/log.do_rootfs.5870

ERROR: Task 7 (/home/srinivasulu/Freescale_BSP/sources/poky/meta/recipes-core/images/core-image-base.bb, do_rootfs) failed with exit code '1'

NOTE: Tasks Summary: Attempted 2427 tasks of which 2426 didn't need to be rerun and 1 failed.

No currently running tasks (2426 of 2428)

Summary: 1 task failed:

  /home/srinivasulu/Freescale_BSP/sources/poky/meta/recipes-core/images/core-image-base.bb, do_rootfs

Summary: There were 3 WARNING messages shown.

Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

please let me know how to resolve the above problem?

0 Kudos
Reply
1 Reply

2,807 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Srinivasulu Reddy,

Would you know how these files were deleted? If they were manually deleted you would need to make a CleanAll and then build again from scratch. As a rule of thumb you shouldn’t delete any file from the folder in which they are deployed. For more information you may read the README that is on the same folder where the images are generated. The problem with deleting these files is that Yocto cannot keep track of what was removed and thus can generate problems.

I would recommend doung a CleanAll of your image and baking again:

$ bitbake –c cleanall <IMAGE>

I hope this helps!